cancel
Showing results for 
Search instead for 
Did you mean: 

bitbake st-example-image-qt ERROR

One&Zero
Associate II

Hi,I execute the following commands according to the wiki:(I am sure accept the EULA)

PC $> DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

PC $> bitbake st-example-image-qt

The following is part of the terminal output :(bitbake st-example-image-qt)

NOTE: Executing Tasks
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: oe_runmake failed
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: Execution of '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.12684' failed with exit code 1:
make: Entering directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found.  Stop.
make: Leaving directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
WARNING: exit code 1 from a shell command.
 
ERROR: Logfile of failure stored in: ../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_compile.12684
Log data follows:
| DEBUG: Executing python function tfaconfig_env
| DEBUG: Python function tfaconfig_env finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8 CROSS_COMPILE=arm-ostl-linux-gnueabi- DEBUG=1 LOG_LEVEL=40 PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 STM32MP_SPI_NOR=1 STM32MP_RAW_NAND=1 STM32MP_SPI_NAND=1 -C ../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/git DTB_FILE_NAME=stm32mp157a-dk1.dtb BUILD_PLAT=../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted AARCH32_SP=sp_min
| make: Entering directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found.  Stop.
| make: Leaving directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.12684' failed with exit code 1:
| make: Entering directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found.  Stop.
| make: Leaving directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| WARNING: exit code 1 from a shell command.
| 
ERROR: Task (../openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 4867 tasks of which 4531 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 10 seconds
 
Summary: 1 task failed:
  ../openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @One&Zero​ 

looks similar to issue in this post :

https://community.st.com/s/question/0D53W00000DHQcwSAH/error-in-building-the-openstlinux-distribution

Fixed by doing bitbake -c cleanall tf-a-stm32mp and relaunch.

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @One&Zero​ 

looks similar to issue in this post :

https://community.st.com/s/question/0D53W00000DHQcwSAH/error-in-building-the-openstlinux-distribution

Fixed by doing bitbake -c cleanall tf-a-stm32mp and relaunch.

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
One&Zero
Associate II

Thank you @OlivierG (ST Employee)​ it worked!