cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any alternative Linux OS for the STM32MP1 system?

DMårt
Lead

Hi!

I'm looking for an alternative Linux OS for the STM32MP1 system. I'm currently using OpenSTLinux, but it's very buggy and have a lack of lots of packages.

Can you recommend a Linux OS or that works with 512 MB Ram + 650 MHz CPU?

I'm planning to only replace the rootfs folder with the new linux distro.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer
2 REPLIES 2
Macdog
Associate III

Several years back we ended up creating a Buildroot distribution, since then I believe that STMicro has offered official buildroot distributions for their ecosystem.    What packages are you looking for that are not available using Yocto or Buildroot?

 

@Macdog 

I have created a Linux distro for stm32mp1 by using buiodroot.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer