cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to program STM32MP1 using UART?

iheb
Associate III

I was wondering if its possible to directly flash the STM32MP1 using UART using the STM32CubeProgrammer ?

if so are there any tutorials that can be followed ?

1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi,

Please see this page: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Using_STM32Programmer_over_UART

Note that programming complete Linux image using UART will be very (very!) long (starter package = ~700MBytes , estimated to ~18 hours). It is recommended for tests purposes and reserved to flash up to uBoot.

It is recommended to use USB.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Hi,

Please see this page: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Using_STM32Programmer_over_UART

Note that programming complete Linux image using UART will be very (very!) long (starter package = ~700MBytes , estimated to ~18 hours). It is recommended for tests purposes and reserved to flash up to uBoot.

It is recommended to use USB.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.