2021-12-27 05:37 AM
I am using MB1407C (stm32mp157x-DK2 extension board with touch-screen) connected to my custom board. When board is booting I am getting the "ST life.augmented" screen on the U-boot and black screen when kernels starts. Also I am getting the telnet commands when I am updating the flashlayout using the CubeMxFlashLoader - so my guess is the DSI connection is working, but why do i get the black screen instead of the Wayland Weston desktop- that is shown when stm32mp157x-DK2 loads up the OS? What am i missing? What is other way to test the DSI connections?
Solved! Go to Solution.
2022-02-10 02:50 AM
Good morning @Arnas Celkys ,
Nice.
I think the probe of the HDMI probably caused an error that was preventing LTDC/DSI to be configured correctly at linux level.
Great that you find the problem.
Regards,
Kevin
2022-01-10 06:32 AM
************* update ************************
Attaching stdout
Starting Weston Wayland Compositor (on tty7)...
[ OK ] Started Sound Service.
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
[FAILED] Failed to start Weston Wayland Compositor (on tty7).
It would appear it fails Weston Wayland Compositor
then I tied:
>>systemctl status weston@root.service
<<
[[0;1;31m*[[0m weston@root.service - Weston Wayland Compositor (on tty7)
Loaded: loaded (/lib/systemd/system/weston@.service; static; vendor preset: disabled)
[[0;1;31m*[[0m weston@root.service - Weston Wayland Compositor (on tty7)
Loaded: loaded (/lib/systemd/system/weston@.service; static; vendor preset: disabled)
[[0;1;31m*[[0m weston@root.service - Weston Wayland Compositor (on tty7)
[[0;1;31m*[[0m weston@root.service - Weston Wayland Compositor (on tty7)
Loaded: loaded (/lib/systemd/system/weston@.service; static; vendor preset: disabled)
Active: [[0;1;31mfailed[[0m (Result: exit-code) since Sun 2020-09-20 10:44:12 UTC; 6min ago
Process: 601 ExecStartPre=/sbin/check-gpu [[0;1;31m(code=exited, status=1/FAILURE)[[0m
Sep 20 10:44:11 stm32mp1 systemd[1]: Starting Weston Wayland Compositor (on tty7)...
Sep 20 10:44:12 stm32mp1 systemd[1]: [[0;1;39m[[0;1;31m[[0;1;39mweston@root.service: Control process exited, code=exited, status=1/FAILURE[[0m
Sep 20 10:44:12 stm32mp1 systemd[1]: [[0;1;38;5;185m[[0;1;39m[[0;1;38;5;185mweston@root.service: Failed with result 'exit-code'.[[0m
Sep 20 10:44:12 stm32mp1 systemd[1]: [[0;1;31m[[0;1;39m[[0;1;31mFailed to start Weston Wayland Compositor (on tty7).[[0m
I seems to indicate to problem of vendor, but this same SD runs on eval-board ok... The custom-board has the same pinout and socket for DSI (double-checked).
Also I have checked the 3V3 for the DSI screen and seems to be stable 3V3.
Not sure should I proceed to tripple check the HW (pcb traces etc.) or issue is on SW...
2022-01-10 06:38 AM
TOP - eval-board schematics
BOT - my custom board shematics
2022-01-10 08:45 AM
>>or issue is on SW...
That you successfully get any image displayed suggests its not a HW connectivity problem.
Start screen suggest that has all the clocking and timing in order for that part (u-Boot ?)
2022-01-11 05:00 AM
Yep it works in U-Boot and goes dark as soon as it starts up kernel, my hunch tells that it is SW too. I will try a few more things and post update :)
2022-02-10 01:13 AM
Hello @Arnas Celkys ,
Do you still need help on this issue?
Regards,
Kévin
2022-02-10 01:54 AM
Good morning, @Kevin HUBER
I just removed HDMI node (because I am not using it at all) as alternative on Kernel device tree - it worked out for me. Thanks!
Regards,
Arnas
2022-02-10 02:50 AM
Good morning @Arnas Celkys ,
Nice.
I think the probe of the HDMI probably caused an error that was preventing LTDC/DSI to be configured correctly at linux level.
Great that you find the problem.
Regards,
Kevin