cancel
Showing results for 
Search instead for 
Did you mean: 

Cross compiling a python program

softcity002
Associate

Hello everyone,

I'm new to the STM32 and Linux environment and have a question.

I am using the STM32MP157d-dk1 and have been following the getting started guide

(see : https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Create_a_simple_hello-world_application ) and how to cross-compile with Developer-Package ( see : https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package#Adding_a_.22hello_world.22_user_space_example  ) and it all works fine. But I'd like to know how to do the same thing but using a .py file instead of .c file from my host machine as i want to mainly use python for my development. 

Thanks for your assistance.

Regards.

1 ACCEPTED SOLUTION

Accepted Solutions

@Ozone wrote:

Not sure if something like 'pip' exists for the MP1s.


Looks like it should:

Solved: Control STM32MP157D-DK1 GPIO with python - STMicroelectronics Community

 

Some "getting started" tips for STM32MP157A-DK1 here:

Solved: Re: STM32MP157A-DK1 can run LINUX and Python code? - STMicroelectronics Community

View solution in original post

4 REPLIES 4

Python is an interpreted language - you don't need to compile .py files.

 

Ozone
Lead III

As Andrew said, Python is an interpreted langauge.

So, you question morphs into - what Python libraries do you need, and if they are available / supported in ST's Yocto package.
Not sure if something like 'pip' exists for the MP1s.


@Ozone wrote:

Not sure if something like 'pip' exists for the MP1s.


Looks like it should:

Solved: Control STM32MP157D-DK1 GPIO with python - STMicroelectronics Community

 

Some "getting started" tips for STM32MP157A-DK1 here:

Solved: Re: STM32MP157A-DK1 can run LINUX and Python code? - STMicroelectronics Community

thanks i will check it out