cancel
Showing results for 
Search instead for 
Did you mean: 

Trying to attach a TI DP83848CVV PHY to STM32MP157 with external 50MHZ

KKett.1
Associate II

Hello,

i'm currently trying to attach a TI DP83848CVV phy to the STM32MP157. We have an external 50MHZ clock which is supplied to the PHY and PA1 (ETH1_REF_CLK).

These are the pinctrl values (generated by CubeMX):

ethernet0_rmii_pins: rmii-0 {
		pins1 {
				pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_REF_CLK */
						 <STM32_PINMUX('B', 12, AF11)>, /* ETH1_TXD0 */
						 <STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
						 <STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
				bias-disable;
				drive-push-pull;
				slew-rate = <1>;
		};
		pins2 {
				pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
				bias-disable;
				drive-push-pull;
				slew-rate = <0>;
		};
		pins3 {
				pinmux = <STM32_PINMUX('A', 7, AF11)>, /* ETH1_CRS_DV */
						 <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
						 <STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
						 <STM32_PINMUX('G', 12, AF11)>; /* ETH1_PHY_INTN */
				bias-disable;
		};
		pins4 {
				pinmux = <STM32_PINMUX('B', 11, AF11)>; /* ETH1_TX_EN */
		};
};

And the ethernet values:

&ethernet0 {
        status = "okay";
        pinctrl-0 = <&ethernet0_rmii_pins>;
        pinctrl-names = "default";
        phy-mode = "rmii";
        phy-handle = <&phy0>;
        max-speed = <100>;
 
        mdio0 {
                #address-cells = <1>;
                #size-cells = <0>;
                compatible = "snps,dwmac-mdio";
                phy0: ethernet-phy@0 {
                        compatible = "ethernet-phy-ieee802.3-c22";
                        reg = <0>;
                };
        };
};

I'm using the default stm32mp157.dtsi:

ethernet0: ethernet@5800a000 {
		compatible = "st,stm32mp1-dwmac", "snps,dwmac-4.20a";
		reg = <0x5800a000 0x2000>;
		reg-names = "stmmaceth";
		interrupts-extended = <&intc GIC_SPI 61 IRQ_TYPE_LEVEL_HIGH>,
							  <&intc GIC_SPI 62 IRQ_TYPE_LEVEL_HIGH>,
							  <&exti 70 1>;
		interrupt-names = "macirq",
						  "eth_wake_irq",
						  "stm32_pwr_wakeup";
		clock-names = "stmmaceth",
					  "mac-clk-tx",
					  "mac-clk-rx",
					  "ethstp";
		clocks = <&rcc ETHMAC>,
				 <&rcc ETHTX>,
				 <&rcc ETHRX>,
				 <&rcc ETHSTP>;
		st,syscon = <&syscfg 0x4>;
		snps,mixed-burst;
		snps,pbl = <2>;
		snps,en-tx-lpi-clockgating;
		snps,axi-config = <&stmmac_axi_config_0>;
		snps,tso;
		power-domains = <&pd_core>;
		status = "disabled";
};

Under linux, a generic phy gets detected, and phytool also shows us data, but wrong values:

Configuring network interfaces... [    6.162488] Generic PHY stmmac-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=stmmac-0:00, irq=POLL)
[    6.183019] dwmac4: Master AXI performs any burst length
[    6.187173] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[    6.194290] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[    6.203155] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[    6.210029] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[    7.276918] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
[    7.283904] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
 
....
root@bytedevkit:~# phytool print eth0/0
ieee-phy: id:0x0000ffff
 
   ieee-phy: reg:BMCR(0x00) val:0000
      flags:          -reset -loopback -aneg-enable -power-down -isolate -aneg-restart -collision-test
      speed:          10-half
 
   ieee-phy: reg:BMSR(0x01) val:0xffff
      capabilities:   +100-b4 +100-f +100-h +10-f +10-h +100-t2-f +100-t2-h
      flags:          +ext-status +aneg-complete +remote-fault +aneg-capable +link +jabber +ext-register

The phy id is wrong: 0x0000ffff and should be 0x20005ca0.

Reading any register outputs 0x0000 and 0xfffff alternating.

The TI DP83848CVV driver is built in into the kernel:

root@bytedevkit:~# zcat /proc/config.gz | grep 8384
CONFIG_DP83848_PHY=y

 I appreciate any help here, thank you.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
PatrickF
ST Employee

Hello,

I'm more on the HW side, so I will cover only those aspects.

I understand you are in this situation: https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#RMII_with_Crystal_on_PHY_-28Reference_clock_-28standard_RMII_clock_name-29_is_provided_by_a_Phy_Crystal-29

Maybe an MDIO bus issue (address, or HW related such as pull-up, voltage, frequency).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
KKett.1
Associate II

Hello Patrick,

yes, "3.3.1 RMII with Crystal on PHY (Reference clock (standard RMII clock name) is provided by a Phy Crystal)" is our situation.

I'm checking tomorrow with our HW engineer and will report back.

What do you mean with mdio address? The reg = <0> value in phy0?

Thank you.

Best regards,

Kevin

KKett.1
Associate II

The PHY now works.

There were two issues:

  1. Missing reset on the PHY reset line (phy just didn't respond)
  2. Wrong phy address

Our pinctrl definitions are now these:

ethernet0_rmii_pins: rmii-0 {
		pins1 {
				pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_REF_CLK */
						 <STM32_PINMUX('B', 12, AF11)>, /* ETH1_TXD0 */
						 <STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
						 <STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
				bias-disable;
				drive-push-pull;
				slew-rate = <1>;
		};
		pins2 {
				pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
				bias-pull-up;
				drive-push-pull;
				slew-rate = <0>;
		};
		pins3 {
				pinmux = <STM32_PINMUX('A', 7, AF11)>, /* ETH1_CRS_DV */
						 <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
						 <STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
						 <STM32_PINMUX('G', 12, AF11)>; /* ETH1_PHY_INTN */
				bias-disable;
		};
		pins4 {
				pinmux = <STM32_PINMUX('B', 11, AF11)>; /* ETH1_TX_EN */
		};
};

And our ethernet definition:

&ethernet0 {
        status = "okay";
        pinctrl-0 = <&ethernet0_rmii_pins>;
        pinctrl-names = "default";
        phy-mode = "rmii";
        phy-handle = <&phy0>;
        max-speed = <100>;
		
        snps,reset-delays-us = <0>, <10000>, <1000000>;
        snps,reset-gpio = <&gpiob 5 GPIO_ACTIVE_LOW>;
        snps,reset-active-low = <1>;
 
        mdio0 {
                #address-cells = <1>;
                #size-cells = <0>;
                compatible = "snps,dwmac-mdio";
 
                phy0: ethernet-phy@1 {
                        reg = <0x01>;
                };
        };
};