2024-09-09 8:35 AM
Hello -
I have the STM32MP257x-EV1 up and running the base image. I have included the layers for the Ethernet switch and TSN. I am trying to understand the embedded Ethernet Switch better. I am working with the assumption that I can plug in two endpoints to ETH1 and ETH3 with no interaction from the MPU and pass ethernet traffic (e.g., ping).
But this does not work from the get-go. Is there something that needs to be done to enable it?
Solved! Go to Solution.
2024-09-18 8:41 AM
This service will not start, nor does running the script manually work.
2024-09-19 3:10 AM
Could you please share a photo of your board (taken from above)
2024-09-19 3:19 AM
2024-09-19 3:24 AM
Ok no issue. Sorry but I don't see what could be the issue. What is the result of these 2 cmd below on your side ?
root@stm32mp2:~# cat /sys/class/net/end*/address
10:e7:7a:e3:b8:e1
10:e7:7a:e3:b8:e2
root@stm32mp2:~# cat /sys/class/net/sw*/address
10:e7:7a:e3:b8:e2
ba:9a:c5:9b:b2:00
ba:9a:c5:9b:b2:01
ba:9a:c5:9b:b2:02
2024-09-19 3:37 AM
I can try rebuilding and re-flashing the board. Is there any place that a complete TSN image is posted that is known-good that I could download and flash? I don't believe the starter/distribution, etc. have these in them/
2024-09-19 4:45 AM
In term of HW all seems ok.
A starter package with tsnswch will be available soon on st.com. I will generate one and share it to you this afternoon.
2024-09-20 9:17 AM
Your image appeared to work fine as far as bringing up the interfaces. Therefore, I am beyond hurdle #1, but still have issues. I will dig into the TSN data some more to understand why my simple use case in the picture above does not completely work.
2024-09-20 10:31 AM
I believe I got this working, thank you for the support.
2024-09-23 12:23 AM
This is good news !!