2020-12-14 04:08 PM
Hi.
I was going to buy STM32MP157C-DK2 but its status NRND(Not Recommended for New Design). So I think to buy STM32MP157F-DK2.
Are they different point is only a clock(650 or 800) of A7 core? What's the difference?
Thank you.
Best regards.
Solved! Go to Solution.
2020-12-15 11:36 PM
I confirm that the major differences are the increased max frequency of the Cortex-A7 cores and the corrections of some HW bugs (Device Rev.Z, see ES0438).
2020-12-15 06:38 AM
Hi @Jungho ,
STM32MP157F-DK2 is assembled with latest STM32MP15 RevZ cut which is the only one available for new product now.
Olivier
2020-12-15 11:36 PM
I confirm that the major differences are the increased max frequency of the Cortex-A7 cores and the corrections of some HW bugs (Device Rev.Z, see ES0438).