STM32 MPUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error: fsbl1 (0x4): invalid address 0x4400 (min=0x80000) during loading flash_layout image to custom STM32MP1 board

Hi!During loading flash_layout image to custom STM32MP1 I've got following error after staring u-boot and truing to load information to partition 0x04 fsbl1:U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000)CPU: STM32MP157DAB Rev.ZModel: STMicr...

ASkri.1 by Senior
  • 1459 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP157C-DK2 Long Turn On Time

I'm working with the STM32MP157C-DK2 dev board and I've noticed that sometimes when powering up the board there is a 20-30 second delay where I don't even see the boot up messages. It's doesn't appear to be U-boot related either. Has anyone else not...

ASuar.1 by Associate III
  • 1557 Views
  • 8 replies
  • 0 kudos

Hello, I am trying to execute a simple ADC program(12bit) in stm32mp157c using trimpot with 10K as input in cube ide. Where output changes only at the voltage level of 3.2v

While changing the value at the trimpot output values is constant(4095) and has no change as soon as when it reaches 3.2V it goes to zero. I am seeing output using uart. ​Please assist me how to rectify it.​

ASuha.1 by Associate
  • 494 Views
  • 1 replies
  • 0 kudos

Resolved! I have been following the instructions on the wiki to set up STM32CubeProgrammer on dk2. It appears I am missing port parameters. What is the correct command line?

I enter STM32_Programmer_CLI -c port=/dev/bus/usb/010/003 (lsusb reports this is correct) -w flashlayout_st-image-weston/trusted/Flashlayout_sdcard_stm32mp157c-dk2-trusted.tsvudev drivers installed, Ubuntu 20.04Warning: Wrong connect parameter:

SLetter by Associate III
  • 1274 Views
  • 9 replies
  • 0 kudos