2022-08-22 6:32 AM
On the default image provided from ST, is there any way to check what color depth is running on it.
I think it is 24bit but not sure. I ran modetest but no option to show this information.
Solved! Go to Solution.
2022-09-22 9:15 AM
Hi Dat Tran (Community Member)
You may have the information you need in https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview
Color format supported using the standard OSTL DV4 on DK board image
at GPU output -> LTDC input
root@stm32mp1:~# modetest -M stm
...
in_formats blob decoded:
AR24: LINEAR
XR24: LINEAR
RG24: LINEAR
RG16: LINEAR
AR15: LINEAR
XR15: LINEAR
AR12: LINEAR
XR12: LINEAR
C8 : LINEAR
root@stm32mp1:~# cat /sys/kernel/debug/dri/0/state
format=XR24 little-endian (0x34325258) -> 24-bit color depth.
Rgds,
Olivier
2022-09-06 9:53 AM
Hi Dat Tran (Community Member)
Do you refer to splash_landscape.bmp? or something else?
$ mediainfo splash_landscape.bmp | grep 'Bit depth'
Bit depth : 8 bits
2022-09-21 4:24 AM
2022-09-21 6:50 AM
Hi @OlivierK
Sorry because "Image" made you think the bitmap image, my image means the img file that write to raw SD.
I mean how to check hardware. I still can't find any solution yet, but we decided to go with 16 bit.
My question is something like, on Window, we can select Display - Setting property .... and we know the display is working on 32bit or 24 bit...
But I could not find anything similar in linux with command line.
I check framebuffer it is 16bit, it doesn't mean Linux is running 16bit.
2022-09-22 1:58 AM
Hi Dat Tran (Community Member)
Sorry your request is still not crystal clear to me.
Do you ask for the graphical framework color deph embedded by default in ST built image, which is the GTK framework for instance. ?
2022-09-22 9:15 AM
Hi Dat Tran (Community Member)
You may have the information you need in https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview
Color format supported using the standard OSTL DV4 on DK board image
at GPU output -> LTDC input
root@stm32mp1:~# modetest -M stm
...
in_formats blob decoded:
AR24: LINEAR
XR24: LINEAR
RG24: LINEAR
RG16: LINEAR
AR15: LINEAR
XR15: LINEAR
AR12: LINEAR
XR12: LINEAR
C8 : LINEAR
root@stm32mp1:~# cat /sys/kernel/debug/dri/0/state
format=XR24 little-endian (0x34325258) -> 24-bit color depth.
Rgds,
Olivier