cancel
Showing results for 
Search instead for 
Did you mean: 

Does nandflash and EMMC of stm32mp157c share the same interface or independent interface?

坤祁.2387
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Hello,

You could find detail information in Documentations (Reference Manual, DataSheet), Application Note (AN5031) or Wiki (e.g. https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview)

To sum-up, we are able to connect simultaneously many interface, if package pin count and your pinout usage allow it (your could quickly test using STM32CubeMx).

e.g. a typical usage similar to STM32MP157C-EV1 board

  • SD-Card 4-bits on SDMMC1
  • eMMC 8-bits on SDMMC2
  • Serial-NOR 4-bits and/or Serial-NAND 4-bits on QUADSPI
  • SLC-NAND 8 or 16-bits on FMC

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
The touch screen part of stm32mp157c-dk2 does not need to be interrupted and reset?