cancel
Showing results for 
Search instead for 
Did you mean: 

Wireless M-Bus (wMbus) and LoRaWAN

alias_bibin
Associate

Hello,

We are in the process of developing a smart meter that will feature dual communication capabilities supporting both Wireless M-Bus (wMbus) and LoRaWAN. Our aim is to use a single chip for this purpose, with the advantage of sharing the same antenna. In this setup, LoRaWAN takes precedence over wMbus in terms of priority.

For selecting suitable components for this project, we are considering chipsets that offer integration of both wMbus and LoRaWAN functionalities. Additionally, we are looking for antennas that provide optimal performance across the frequency bands used by both protocols.

Could you please suggest specific chipsets and antennas that align with these requirements?

Thank you.

3 REPLIES 3
STTwo-32
ST Employee

Hello @alias_bibin and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you take a look at the STM32WLE5/E4 and STM32WL55/54 lines that enable the design of cost-efficient connected devices running LoRaWAN and W-MBUS certified stacks or other proprietary or standardized sub-GHz protocols.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

alias_bibin
Associate

Hello, 
please find the requirements :

  1. Sharing the same antenna with wMbus and LoRaWAN protocol.
  2. Transmission frequency

     868MHz

    Protocol

    Sigfox Verified & Sigfox Ready

  3. LoRaWANTM  certified with a communication profile of Class “A”  "Aloha"

  4. Lowrawan must have higher priority over walkby.
  5. need to use the product in the Germany.

is this chip support these 2 protocols? is any communication error happen while try to transfer data by these two protocol by same time?

 

Billy OWEN
ST Employee

Hi @alias_bibin 

 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

 

Regards,

Billy