‎2021-05-21 07:20 AM
I'm using the STM32CubeIDE (Version: 1.6.1) and I've installed the package for the family STM32WB (rel 1.11.1) but into the section 'Example Selector' I don't find any example for this board. I don't understand what's the issue. What I should do for import some example to start to work correctly with this board?
Regards,
Giampietro
‎2021-05-21 07:36 AM
Works for me so ? Note: if you don't have package already STM32CubeIDE is installing it for you.
Got a try to refresh your local database "Help > Check For Target Selector Device Database Update" then "Refresh" and open back example selector: is it better ?
As you have got package already you can always rely on "File > Open Project From File System" looking at STM32Cube_FW_WB_V1.11.1\Projects but be aware then your project remains local to the pack what's a way but less convinient according to me than official example import feature.
‎2021-05-21 07:54 AM
I've this example:
but I need example for the board STM32WB5MM :
For this board I find no example. Could you help me for understanding where is the problem?
Thanks
Giampietro
‎2021-05-21 08:04 AM
You're right sounds no example as part of example selector if WB5MM.
Looking at the pack/ STM32Cube_FW_WB_V1.11.1\Projects\STM32WB5MM-DK sounds some examples but all of those are IAR only supported :sad_but_relieved_face: at that time ...
Let's hope CubeIDE ones are coming if next release.
Do you need a specific one of those example ?