2022-02-08 1:29 PM
The operating temperature range for the above MCU is -40 to 85 deg C (105 deg C junction). Does it mean that the maximum temperature for soldering is 105 deg C, or does it just mean that the MCU will shut down at 105 deg C? I would appreciate it if you refer to any official application note.
Solved! Go to Solution.
2022-02-08 6:35 PM
85C (105C junction) is the max operating temperature. Junction temperature is what actually matters here. Beyond that range the behavior is no longer guaranteed.
Soldering will need to be quite a bit hotter.
2022-02-08 6:35 PM
85C (105C junction) is the max operating temperature. Junction temperature is what actually matters here. Beyond that range the behavior is no longer guaranteed.
Soldering will need to be quite a bit hotter.
2022-02-09 6:51 AM
Thank you