cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F765IIK6 Reflow Problems

MBake
Associate

We are using STM32F765IIK6 176 pin 10x10 0.6mm UFBGA, die rev "Z". Whilst processing these through SMT solder reflow (using an 8 zone forced air convection oven) we had a number of these devices failing, due to the substrate of the BGA package dishing causing solder shorts & opens under the device.

We have followed the J standard pre bake & storage process for these devices (MSL 3) and have profiled the board and device, so as not to exceed the upper reflow profile, as stated at 260°C on the Materials Declaration Form for the device. The actual device peak temperature during soldering was 255°C with a ramp rate of less than 3°C / Second.

We are using a Halogen Free Ultra Life Solder Paste SAC 305 (Sn96.5/Ag3.0/Cu0.5).

We have tried different date code STM32F765IIK6 devices through the process and some are more suspectable to failing than others. All have been pre baked and procesed in the same way.

We found that lowering the peak reflow temperature reduced the dishing affect and the number of failures, but this created problems with other devices on the board not correctly soldering (i.e. the NiPdAu plated parts).

Please can you ;

i: Clarify the reflow profile limits for this device and package substrate - i.e. is the Material Declaration Form parameters correct.

ii: Whether you have other reported failures for this device / package type - and if so any corrective action to resolve issue.

Thanks

Martin

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

This really isn't the venue. You should work with your local sales office and the FAE assigned to your account to resolve the issue, and get your information in front of engineers with specific understanding of packaging and fabrication issues.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..