2023-03-30 4:57 AM
While reverse engineering a demo application from ST / Seeed ( Seeed-Studio/LoRaWan-E5-Node at qian (github.com)), I started monitoring all commands and register access from the MCU to the embedded SX126.
I see there are writes to register:
WR [08E2]:0C
WR [08E5]:20
Those registers are not mentioned in the datasheet from Semtech, nor the STM32WLE5 datasheet from ST…
What is the purpose of those registers ?
Why is the SW writing those values ?
Why is this not in the datasheet ???
2023-03-30 9:52 AM
Got an answer from Semtech forum :
The registers you mentioned are used in sx126x_get_random_numbers function.
They are altered to modify some internal logic allowing random numbers to be generated from RF noise without being impacted by a potential jammer.
2023-03-30 10:17 AM
/*! * The address of the register used to disable the LNA */
#define SX126X_REG_ANA_LNA 0x08E2
/*! * The address of the register used to disable the mixer */
#define SX126X_REG_ANA_MIXER 0x08E5
Clearing bits 0 and 7 respectively.
Did they point to any register level documentation?
2023-03-30 10:20 AM
Not yet : here is a link to the topic on Semtech forum : What does SX126 register 0x8E2 and 0x8E5 do? - Semtech Transceivers - FORUM