cancel
Showing results for 
Search instead for 
Did you mean: 

WB55 USB Dongle Not Seen by CubePgmr In Windows

GRama.2
Associate III

Hello

I have tried to update the FUS, BLE Stack, and the default client app on the dongle.

I have now done this several times, with the Clent App not doing what the UM says.

But the issue now is that the USB Dongle in Boot0 mode is not seen by windows (--> Cube Programmer).

If I move the switch to std mode, no difference. Only the green LED lights on the dongle.

Have I bricked the device? or is there a process to bring it back.

Thank you.

Giri

7 REPLIES 7
STTwo-32
ST Employee

Hello @GRama.2 

Have you verified that the BOOT0 switcher SW2 is set to 1 and connect to the Cube Programmer using the USB mode:

STTwo32_0-1718299434418.png

The dongle can be connected and programmed only using the USB mode (No embedded ST-LINK on the Dongle).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

GRama.2
Associate III

Yes, I have verified SW2 is set to 1.

GRama.2
Associate III

Apologize, somehow I had clicked on Accept Solution by mistake and am unable to undo 

SW2 was/is 1

 

Are you cinnecting under USB or DT-Link.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Connected via USB using CubeProgrammer v2.16.0

Just to circle back, with the state of the Dongle above - is it a brick?

Thanks

Giri

I can't confirm this. Can you try using another Dongle to ensure about the source of the problem. (on my side everything works fine).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.