2024-10-15 2:42 AM
Dear All,
Our work is focused on the STM32 WL55JC1 board!
What we would like to achieve is use its RF transceiver as W-MBus.
It seems that WL55 is suitable for WM-Bus since its transceiver supports the appropriate frequencies and modulations for such purpose.
Still I was not able to find any example code so that WL55 can be used with WM-Bus and trying to do it from scratch seems difficult for someone not that experienced.
Looking at X-CUBE-SUBG1 package there are lots of examples for WM-Bus but they target the SPIRIT1 and S2-LP transceivers.
I was thinking to manually integrate the WM-Bus example code (X-CUBE-SUBG1) to WL55 but I guess it will not work out-of-the-box since it is equipped with another transceiver (I think Semtech).
I wanted to ask if anyone is aware of an example code to use WM-Bus with WL55 or if anyone can provide a suggestion/help to this direction!
Thank you!
Solved! Go to Solution.
2024-10-15 3:24 AM
Hello @Dimitrios Bako
the Wireless M-Bus for the STM32WL is available from our partner StackForce as a commercial version only, as you can find on their website.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-15 3:24 AM
Hello @Dimitrios Bako
the Wireless M-Bus for the STM32WL is available from our partner StackForce as a commercial version only, as you can find on their website.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-15 5:23 AM
Dear STTwo-32,
Thank you very much for the quick reply!
Best regards,
Dimitrios Bakoyiannis