cancel
Showing results for 
Search instead for 
Did you mean: 

W-MBus Example Code for WL55JC1

Dimitrios Bako
Associate II

Dear All,

Our work is focused on the STM32 WL55JC1 board!

What we would like to achieve is use its RF transceiver as W-MBus.

It seems that WL55 is suitable for WM-Bus since its transceiver supports the appropriate frequencies and modulations for such purpose.

Still I was not able to find any example code so that WL55 can be used with WM-Bus and trying to do it from scratch seems difficult for someone not that experienced.

Looking at X-CUBE-SUBG1 package there are lots of examples for WM-Bus but they target the SPIRIT1 and S2-LP transceivers.

I was thinking to manually integrate the WM-Bus example code (X-CUBE-SUBG1) to WL55 but I guess it will not work out-of-the-box since it is equipped with another transceiver (I think Semtech).

I wanted to ask if anyone is aware of an example code to use WM-Bus with WL55 or if anyone can provide a suggestion/help to this direction!

 

Thank you!

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Dimitrios Bako 

the Wireless M-Bus for the STM32WL is available from our partner StackForce as a commercial version only, as you can find on their website.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Dimitrios Bako 

the Wireless M-Bus for the STM32WL is available from our partner StackForce as a commercial version only, as you can find on their website.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Dear STTwo-32,

Thank you very much for the quick reply!

Best regards,

Dimitrios Bakoyiannis