2021-03-03 6:52 AM
Hello, after playing a bit with P-NUCLEO-WB55 pack I bricked the board.
The board is visible by Cube Programmer in DFU mode. Programmer can see the ST-Link but ST-Link does not detect the target.
Thanks.
2021-03-04 5:49 AM
There is no FUS. The whole MCU is erased.
I'm trying to flash 1.11.0 at the address 0x080EC000 according to Release Notes.
BTW, it looks like ST-Link is trying to upload first something temporary at 0x0800_0000:
13:12:59 : Opening and parsing file: 0x495_FUS_Operator.bin
13:12:59 : File : 0x495_FUS_Operator.bin
13:12:59 : Size : 11584 Bytes
13:12:59 : Address : 0x08000000
I would say it's pretty tricky as it would erase a piece of application FW if it were programmed to flash before. Isn't it?
2021-03-04 6:04 AM
To clarify: I'm running from the FUS screen of the Programmer and not from the "Erasing & Programming".
(Not sure what is the difference between them)
2021-03-04 6:58 AM
>> BTW, it looks like ST-Link is trying to upload first something temporary at 0x0800_0000
>> I would say it's pretty tricky as it would erase a piece of application FW if it were programmed to flash before. Isn't it?
It's normal, it is the way it is working and the F.U.S is not supposed to be updated so often.
Please try to update the FUS with version v1.1.2, which is in STM32WB firmware package V1.10.1 / 15-January-2021
https://www.st.com/en/embedded-software/stm32cubewb.html
Please read: