cancel
Showing results for 
Search instead for 
Did you mean: 

How to run bootloader on bricked STM32H7 Discovery kit?

Clem1
Associate III

I have recently bricked my STM32H7 discovery kit by trying to select the M4-only boot option, but I am no longer able to connect the debugger. I have had a similar problem with the Arduino Giga board but I managed to "unbrick" it by running a bootloader and pressing the "BOOT0" button. According to the STM32H7 manual, the bootloader should is loaded by a combination of a high BOOT0 and the status of certain option bits (over which I obviously do not have any control any longer). For the Discovery board, I have soldered in a button that shorts out R192 and which I then press while powering up / resetting, but neither the STM32CubeProgrammer nor the ST flash loader demo is able to connect through the UART (via the in-built ST link programmer). Do you have any advice on how to start the bootloader? Surely there must be a way to save that board? Do I need to use a different USART port?

Many thanks,

Clem

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Clem1
Associate III

Hi all. I have found the answer myself. Apparently, the SWD channel needed to be changed to channel 3, which accesses the M4 core directly, see STM32H747I-DISCO bricked after unchecking ECM7 bit on STM32CubeProgrammer

View solution in original post

4 REPLIES 4
Clem1
Associate III

Hi all. I have found the answer myself. Apparently, the SWD channel needed to be changed to channel 3, which accesses the M4 core directly, see STM32H747I-DISCO bricked after unchecking ECM7 bit on STM32CubeProgrammer

+1 Multiple cores, connecting to the functional core

The BOOT0 HIGH and power cycling trick is primarily for the unbricking in the LDO/SMPS cases

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for clarifying the point about the BOOT0 input. I have been able to unbrick the platform and run a simple blinky-blink demo (35) Getting started with STM32 Dual Core CPUs || STM32H745 || How to DEBUG - YouTube . Despite the simplicity I could only make this work while debugging, once I disconnected from the debug session the MCU would do nothing after a reset. It was as if the debugger transferred the code into RAM and did not program the flash memory. I will raise this question separately since it is not really related to the bricking.

Make sure BOOT0 is pulled down in the normal case.

Usually code does run, watch for places where it gets hung up in while(1) loops of silent death.. ie Error_Handler(), HardFault_Handler(), etc

Make sure both cores have their own routines which output diagnostic/telemetry data that's actionable.

Minimally have some GPIO which can be brought up in the respective Reset_Handlers, and toggled, adjusted as a means of determining functionality absent the debugger.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..