cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to start FUS

ATaba.1
Associate II

I am using the STM32WB55RG MCU, Bluetooth feature with stack version 1.13.0 and FUS version 1.2.0. Everything was working normal until I tried doing the firmware upgrade of stack from v12.0 to v13.0. I am not able to perform FUS related operations. The version reading shows 0.0.0 for FUS. And following is the log when I hit "Start FUS"

 11:09:47 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

 11:09:47 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

 11:09:47 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

 11:09:47 : Warning: Option Bytes are unchanged, Data won't be downloaded

 11:09:47 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

 11:09:47 : Memory Programming ...

 11:09:47 : Opening and parsing file: 0x495_FUS_Operator.bin

 11:09:47 :  File     : 0x495_FUS_Operator.bin

 11:09:47 :  Size     : 8 KBytes

 11:09:47 :  Address    : 0x08000000 

 11:09:47 : Erasing memory corresponding to segment 0:

 11:09:47 : Erasing internal memory sectors [0 1]

 11:09:47 : Download in Progress:

 11:09:47 : File download complete

 11:09:47 : Time elapsed during download operation: 00:00:00.272

 11:09:47 : Application is running, Please Hold on...

 11:09:47 : Reconnecting...

 11:09:47 : Reconnected !

 11:09:51 : Reconnecting...

 11:09:51 : Reconnected !

 11:09:51 : Error: FUS_STATE_ERR_UNKNOWN

 11:09:51 : Start FUS failed !

 11:09:51 : Error: Start FUS Operation Failure! Please, try again

Following is OB info attached. Cube programmer version I am using is : v2.9.0

What could be the issue, please let me know how to resolve FUS and start wireless stack successfully ?

Thanks.

Arshiya Tabassum

@bponnanavenkat@actalentservices.com

27 REPLIES 27

I tried this binary but it did not work.


_legacyfs_online_stmicro_images_0693W00000bk3l0QAA.png

why this address?
_legacyfs_online_stmicro_images_0693W00000bk3jqQAA.png

Remi QUINTIN
ST Employee

ESE option byte is unchecked meaning tis board is not populated with a FUS. So no way to use it to load any new version of FUS or wireless stack.

This board should be a very old one as only the very first boards were shipped unsecure.

Remi QUINTIN
ST Employee

When a board is secure (ESE bit set), the FUS version is written at address 0x20030030 when the board is connected via USB in DFU mode.

yes, it is old. So there is no way to upgrade FUS?

Remi QUINTIN
ST Employee

Unfortunately, not.

You can still use it to load an application but without RF functionality.

:-(

Thanks then for answer.