cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to build example projects NUCLEO-WB05KZ

utelettronico2
Associate

STM32CubeIDE

Version: 1.12.1
Build: 16088_20230420_1057 (UTC)

I am trying to use one of the examples from the STM32Cube_FW_WB0_V1.1.0 package, but I am unable to build any of them.

After importing the project into STM32CubeIDE (I have tried BLE_Beacon and BLE_Power_Consumption), I attempt to build it, but I get the error shown in the image.

Cattura.PNG

At this point, I have to force close CubeIDE from the Task Manager because the program gets stuck with hundreds of error windows popping up.

I'm obviously missing a step, but I can't figure out which one. Has anyone encountered this issue before?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @utelettronico2 

The STM32CubeWB0 has been supported on the V1.16.0 of the STM32CubeIDE. So, could you please try to use the last version of the STM32CubeIDE (V1.18.0).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Souhaib MAZHOUD
ST Employee

Hello @utelettronico2 

The CubeIDE-1.12.1 does not support WB0 series, please upgrade your CubeIDE to the latest version.

BR,

Souhaib

STTwo-32
ST Employee

Hello @utelettronico2 

The STM32CubeWB0 has been supported on the V1.16.0 of the STM32CubeIDE. So, could you please try to use the last version of the STM32CubeIDE (V1.18.0).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.