cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to access the CFG_HW_USART1_DMA_TX_SUPPORTED parameter on Nucleo-STM32WB55 for BLE use

Curious_Intern
Associate II

Hello,

I'm a beginner on CubeIDE but I want to learn how to use the BLE from the STM32WB55 Nucleo Board. I've been following several tutorials throughout the web, from ST and others, such as https://www.youtube.com/watch?v=i10X4Blr8ns or https://www.youtube.com/watch?v=QbeJFj9LNvc. I do everything as told, but my problem appears when I try to set the BLE. There I have disable everything, except from the Custom Template parameter:

Curious_Intern_0-1708613348700.png

Then, in Configuration, I enable CFG_HW_USART1_ENABLED which is supposed to give me access to the next parameter: CFG_HW_USART1_DMA_TX_SUPPORTED but this one stays unaccessible as shown here: 

Curious_Intern_1-1708613561267.png

 

I've followed the red message to ensure that everything was right, but the previous steps already checks those requests.

Does anyone has any hint for me? 
I would appreciate it a lot. 
Thanks in advance!

1 REPLY 1
ghrairim
ST Employee

Hello @Curious_Intern

First you should continue the BLE Advertising to complete data located in the app_conf.h ,  ble_conf.h and app_ble.c . After that, the next step is the USART setup so go to USART interface and select Asynchronous Mode , then you should to go to DMA settings tab to add the USART1_TX so then click on USART1_TX line to show DMA Request Settings Also go to NVIC Settings tab and enable USART1 global interrupt After that go to STM32_WPAN setup interface and select the configuration tab and enable the application traces, set CFG_DEBUG_TRACES_UART on hw_uart1 .

This WIKI can help you ( https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_STM32CubeMX ). 

Best Regards,