2019-05-13 08:42 PM
Sorry for such a newbie question....
I can connect and debug in CubeMX, was trying to get a project started in CubeIDE.
I can select the CPU, but I don't see the board package. Is there some initialization I might be missing?
IDE connects, then pausing debug, it is in the fault loop.
Log:
------ Switching context -----
Hardware watchpoint supported by the target
SWD frequency = 4000 kHz
ST-LINK Firmware version : V2J33S25
Device ID: 0x495
PC: 0x8004608
ST-LINK detects target voltage = 3.26 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
handle_vCont_c, continue thread
ST-LINK device status: RUN_MODE
handle_vCont_t, Halt thread
ST-LINK device status: HALT_MODE
/* Suspend Issued */
TraceCaptureStart and SWV event set to APP_FALSE (0)
NVIC_DFSR_REG = 0x00000009
Solved! Go to Solution.
2019-05-14 04:21 AM
2019-05-14 04:21 AM
2019-05-14 07:24 PM
Thank you so much for the link that has the hint!!!!!!
I have it working now from the info in the other thread. Editing the both! ld files with the correct address.