2023-05-29 04:26 AM
Hello,
Im trying to add USB support to the MAC 802.15.4 FFD example by copying the HID Standalone example. The code is building and the FFD example is still working with another nucleo running the RFD example, but the WB55 Nucleo is not recognised or enumerated as a USB device on a PC.
Steps performed:
I don't know where to start debugging the USB peripheral. Any help is appreciated.
Best regards,
Taco
2024-05-23 11:41 AM
Hi @TEelm.1
Do you mean you cannot enumerate WB55 Nucleo using this example ? STM32CubeWB/Projects/P-NUCLEO-WB55.Nucleo/Applications/USB_Device/HID_Standalone at master · STMicroelectronics/STM32CubeWB (github.com)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.