2020-04-09 9:23 PM
I test it on P-NUCLEO-WB55 kit board which without any other devices connected on it with the official examples "PWR_STOP2_RTC" ,and I did test it as the readme.txt file tell me(remove all jumpers on JP5, and test the current on the JP2), but the result is near 116uA.
Also I have test the standby mode with the "PWR_STANDBY_RTC" examples, the result is about 0.2uA which is ok.
So what's the matter would it be with the STOP2 mode about the big current?
Looking forward to your reply.
Thanks.
xiaodong.zhao
2020-04-13 4:20 AM
Hello , Is there anyone can give any suggestion please?
2020-04-14 11:22 AM
Set DBGMCU_CR to zero before entering low-power mode.
2020-04-15 12:43 AM
Hi Piranha:
I've tried that, but it doesn't work.
Thanks.