2024-05-29 3:27 AM
Hello ST Community,
I am currently working with a STM32WL 55JC and I need assistance with setting the sync word for both the transmitter and receiver. Here are the details of my setup.
Here I have configured my module to USE_MODEM_LORA and these are the packet params of the USE_MODEM_LORA
This below is the set sync word function whish is present in the radiodriver.c file
here is the another function which is
I want to use the private syncword how do i do that when i use USE_MODEM_LORA.
2024-06-05 8:11 AM
Hello @Shivaprasad
To configure a private syncword in a STM32WL LoRa project when using USE_MODEM_LORA, you would typically follow these steps:
Set the Packet Type to LoRa: Use the Set_PacketType() function to set the packet type to LoRa.
Define the Frame Format: Use the Set_PacketParams() function to define the frame format according to your requirements.
Set the Sync Word: Use the Write_Register() function to define the synchronization word in the associated packet type SUBGHZ_xSYNCR(n) registers. The synchronization word for private networks is different from the public LoRa network sync word.
Set the Network to Private: Use the RadioSetPublicNetwork() function to set the network to private by passing false as an argument.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.