2020-08-16 9:38 AM
Hi.
Using STM32CubeProgrammer I load last stm32wb5x_BLE_Stack_light_fw.bin, but when after that I try to run command -fwdelete, I get an error : "FUS_NOT_RUNNING".
I attach log file becose Idont understand whot is this.
But me application work fine and I see that stack is a last version.
Please help whot may bee .
I send call:
STM32_Programmer_CLI.exe -c port=usb1 -fwdelete -vb 3
2020-08-27 2:39 AM
Hi, Remi.
Yes, my custom application and bootloader uses BLE stack and no any problems.
Application and bootloader can advertise and connect, transfer any data by custom characteristics.
How ti correct write data to address ?
I use:
STM32_Programmer_CLI.exe -c port=usb1 -w32 0x5800040C 0x00008000
but get error:
2020-08-27 2:51 AM
Could you download all the sections of the options bytes or call the command STM32_Programmer_CLI.exe -c port=usb1 -ob displ and give me the log?
2020-08-27 2:53 AM
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 2058387A3036
FW version : 0x011a
Device ID : 0x0495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x1fff8000
Size : 128 Bytes
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒ 0%
██████████████████████████████████████████████████ 100%
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)
User Configuration:
nBOOT0 : 0x1 (nBOOT0=1 Boot from main Flash)
nBOOT1 : 0x1 (Boot from Flash if nBoot0=0 otherwise system memory)
nSWBOOT0 : 0x1 (BOOT0 taken from PH3/BOOT0 pin)
SRAM2RST : 0x1 (SRAM2 is not erased when a system reset occurs)
SRAM2PE : 0x1 (SRAM2 parity check disable)
nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
WWDGSW : 0x1 (Software window watchdog)
IWGDSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
IWDGSW : 0x1 (Software independent watchdog)
IPCCDBA : 0x0 (0x0)
Security Configuration Option bytes:
ESE : 0x0 (Security disabled)
SFSA : 0xD6 (0xD6)
FSD : 0x0 (System and Flash secure)
DDS : 0x1 (CPU2 debug access disabled)
C2OPT : 0x1 (SBRV will address Flash)
NBRSD : 0x0 (SRAM2b is secure)
SNBRSA : 0xF (0xF)
BRSD : 0x0 (SRAM2a is secure)
SBRSA : 0xA (0xA)
SBRV : 0x35800 (0x35800)
PCROP Protection:
PCROP1A_STRT : 0x1FF (0x80FF800)
PCROP1A_END : 0x0 (0x8000800)
PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
PCROP1B_STRT : 0x1FF (0x80FF800)
PCROP1B_END : 0x0 (0x8000800)
Write Protection:
WRP1A_STRT : 0xFF (0x80FF000)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0xFF (0x80FF000)
WRP1B_END : 0x0 (0x8000000)
2020-08-27 3:08 AM
Remi, tell me please, we have a many chips WB55 with REV6.
Our chips marking:
ST (e3)
STM32WB55
REV6
7B A6G 9R Y
PHL GQ 945
ARM 31
It is a normal chip ? (we haven't used it yet)
And what a last revision of chip ?
2020-08-27 3:28 AM
Ok nothing wrong regarding the option bytes except this puzzling ESE set to 0.
Regarding the marking, I would be interested in the one on the failed chip.
I'll come back to you with information on the one above.
2020-08-27 3:33 AM
Marking of failed chip:
STM32WB55
RGV6U
78 A4L 9R Y
PHL 3R 8 44
ARM 64
2020-08-28 2:33 AM
Both markings show valid secured devices.
So I would consider this failed part as not usable anymore.
Could you send this chip back to us? We will perform further analysis.
2020-08-28 6:44 AM
Hi, Remi.
This chip is sealed from the nucleo board and soldered to our custom board.
I can unsolder it, but tell me where to send it? Please write the complete address for sending it.
Thanks.
2020-08-28 7:04 AM
Remi QUINTIN
STMicroelectronics Grenoble2 SAS
12 Rue Jules Horowitz 38019 Grenoble FRANCE
We can send you a STM32WB55 Nucleo pack as an exchange if you want.
2020-08-28 7:40 AM
Ok, thanks, Remi.
On Monday I will do the same research with other chips.
Maybe it will be the same with them.
Then I'll send you the problem chip.