2024-07-26 06:09 AM
I'm using a STM32WLE5cc inside a RAK3172 (TCXO) module on a custom board. I have custom firmware developed in the STMCube IDE. So, my join request is seen on the gateway, and the gateway sees a join accept from the server. Unfortunately the joined event is not seen on the STM. I'm using the endpoint template as a framework.
What is the best procedure to track down where the fault lies?
2024-07-26 01:09 PM
Even though the interrupts for radio rx & preamble are being setup, they are never firing. Radio tx fires ok, so the interrupt handler is ok.
2024-09-13 10:13 AM
Hello @SLevi.1
This module is using an STM32WL with the implementation of a Third party. So, I think it will be really a good idea to look for support on the Forum of the Third-Party.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.