cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL55JC LoRaWAN Working Only on Dual-Core for FUOTA

karthiksb
Visitor

I'm working on a project with the STM32WL55JC microcontroller. Before testing the LoRaWAN_FUOTA_DualCore application, my LoRaWAN setup was functioning correctly with all example applications.

However, after flashing the LoRaWAN_FUOTA_DualCore application, I noticed that only this application is working. While other applications like LoRaWAN_FUOTA, LoRaWAN_End_Node, and LoRaWAN_End_Node_DualCore are functional in terms of peripherals, my device is unable to connect to the LoRa gateway.

Could you help me understand why it’s only working with the LoRaWAN_FUOTA_DualCore application?

0 REPLIES 0