2024-11-19 5:45 AM - edited 2024-11-19 11:53 PM
I am trying to detect my stm32wba52cg bare chip with my developed custom PCB board with onboard stlink as external programmer from a discoveryboard but its showing this msg-
Can not connect to target!
Please select "Connect Under Reset" mode from Target->Settings menu and try again.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
No target connected.
this are my connection for programming my wba52 controller-
discovery stlink stm32wba52
swdio swdio
swclk swclk
nrst rst
3.3 (from discovery board) 3.3
gnd gnd
Below is my schematic attached:
I have exposed all the pins.
Solved! Go to Solution.
2024-12-02 10:57 PM
Hello @suvendusahux
This is a new issue. please close this post by selecting the answer to your original post as best answer. After that create a new post with a good description of the behavior. This will give your post more visible for others who have the same issue and may have a quick solution.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.