2024-01-30 08:05 AM
How do I connect x-nucleo-lpm01a with STM32WB5MM-DK to test power?
I am using the RF module from STM32WB5MM-DK and not the one from P-NUCLEO-WB55.
I know that there is a video for P-NUCLEO-WB55. Is there a video/guide for STM32WB5MM-DK as well?
Solved! Go to Solution.
2024-01-31 02:38 AM
Hello @DS.4
To connect the STM32WB5MM-DK to the X-Nucleo-lPM01A, you have to:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-31 02:38 AM
Hello @DS.4
To connect the STM32WB5MM-DK to the X-Nucleo-lPM01A, you have to:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-20 04:55 AM - edited 2024-03-20 04:55 AM
Connect the Pin 1 of the CN14 of the X-Nucleo-lPM01A to a GND pin of the STM32WB5MM-DK.
Is there an available pin or do I need to solder one?
2024-03-20 05:26 AM
Hello @DS.4
There is GND pins on the Arduino connector:
And also, on the ST Mod+ connector:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-20 05:52 AM
- only works with ST link connected, otherwise its just show ~1mA constant
- I get this offset of 250uA when enters sleep ( I guess because of above?) , using BLE_HearRateFreeRtos example for P-NUCLEO-WB55
2024-03-20 07:28 AM
How can I power it from external source to validate?
2024-03-21 04:37 AM
Can I reach 3uA same as in P-NUCLEO-WB55