cancel
Showing results for 
Search instead for 
Did you mean: 

Is there firmware to support EMC testing of an STN32WL55JC based LoRa device?

AMcCl.1
Associate

Specifically I need to be able to set continuous transmission at full power using each end of the band.

 

I also need to perform immunity tests, but I don't know how to get information out of the device at a suitable rate, short of having a physical cable on a UART, which would mess with the normal configuration, affecting EMC behaviour.

 

Has anyone done this before?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0