2022-10-17 10:24 PM
When a gpio detects an external event (triggered by the falling edge), the server sends a 15 byte notification. I use stm32wb55rgv6 to collect ADS1299 (ADC) data. The sampling rate is 1K (that is, 1000 falling edge triggers). The server should send 1000 15 byte notifications per second, but in fact, I can only receive 180 15 byte notifications.
Under the same peripheral configuration, I will store the collected data to the SD card. There is no error in the data. However, when I use Bluetooth, the data will be missing a lot.
2022-11-07 7:13 AM
Hello,
The number of notifications send each second depend of the connection interval and the CE length used in your application.
Best Regards
2022-11-07 5:25 PM
Thank you.