cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32wb55rev6 communication with custom zigbee3 client

niko27
Associate II

I have a zigbee 3 client working on channel 11 . But It was developed by some other person who was not in touch anymore .. the issue is I need to develop a project that only read a temperature data and frequency value and send those 2 values over zigbee client that connected on a PC through a TTL .. I don't have any idea about zigbee communication procedure and API s . And also I didn't got any source where I can easily understand the process .. can  anybody give. Some guidance to do th process

1 REPLY 1
STTwo-32
ST Employee

Hello @niko27 

I suggest you to take a look to the following application notes:

Also, you can also refer to this wiki and all his sub-categories for more informations.

Then, you can refer to the Zigbee examples of the STM32WB cube package.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.