‎2024-05-28 9:16 AM - last edited on ‎2024-05-28 9:28 AM by Tesla DeLorean
Hello everyone,
The last few days I have been trying to get Zigbee working on my STM32WB55CGU6 and I can now switch on and off a light! But the more difficult thing to get working is the WindowCover. Below you will find the image where my STM32 has connected to home assistant and I can turn the led on and off with the top switch. The problem I now have is sending the other attributes in particular the position. Below you will find my app_zigbee.c file
‎2024-05-29 3:24 AM
Hi @Hesseltjuuh,
The implementation of the cluster seems correct to me.
What is going wrong when you send window commands ? Do you receive the commands through the defined callbacks ? Is there any errors reported?
Please share the Wireshark capture to analyze further your case.
Best regards,
Ouadi
‎2024-06-22 7:32 AM
Allright I've ordered a Zigbee sniffer since it's still not working. I have figured out however how to get to the logs of homeassistant and maybe it's something similar to Wireshark. Also I never get into the callback function.
The log is linked below. You can ignore the 'SmartCandle' and the 'Temperature sensor'
‎2025-01-13 6:21 AM
I still haven't tackled this problem and it's bugging me. I've bought a CC2531 Zigbee sniffer and can now see what's being communicated between my home assistant and the stm32 chip. When I change the position in the picture below a command is send out which you can see in the other picture.
I can see that the status is 'Unsupported Cluster Command' but I think i got everything setup right. The device got interviewed so everything should be set correct right?