STM32WB55CCU6 low energy Bluetooth microcontroller without USART interface
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-06 5:10 AM
I am using the STM32WB55CCU6 low energy Bluetooth microcontroller. As I am not using the USART interface and don't need to support a Real Time Calendar clock, I didn't attach an external low frequency crystal resonator. However, I am wondering whether this was a mistake as the BLE Bluetooth interface requires a low frequency clock [ RTC ] and it doesn't seem possible to use the internal low frequency clock [ LSI ] - disabling RTC also disables the RF section in the .ioc file.
Is there some form of work-around that allows for the use of the internal low frequency oscillator ?
@JBlac.1
- Labels:
-
BLE
-
RTC
-
STM32WB series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-11 1:55 AM
Hello,
If you don't have an external low frequency crystal resonator, you should use HSE/1024 clock as input for RF system wakeup clock. The BLE doesn't require RTC to work, RTC is required in the application for the timer for example.
Best Regards