2019-07-06 04:14 AM
Hello,
I have STM32WB set from workshops that I borrowed from my work.
The problem is both pcbs are not recognised in DFU mode. I connected stm32f4-discovery and it's recognised correctly.
I'm Linux Mint 19 user and I have followed CubeProgrammer's installation manual. I did the same on Windows 10 with the same effect.
On nucleo board I connected pins 5-7 and USB MCU SOURCE.
On dongle board I set switch position to BOOT.
What is the problem? It's look like both of pcbs don't have bootloaders.
Do I need to buy a new stm32wb development kit or can I program a new bootloader file?
Can I flash the Wireless Coprocessor Binary without DFU? I want to turn on BLE examples, but they didn't work.
--- stm32f4-discovery ---
marek@marek-desktop:~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin$ ./STM32_Programmer_CLI -l
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
===== DFU Interface =====
Total number of available STM32 device in DFU mode: 1
Device Index : USB1
USB Bus Number : 001
USB Address Number : 003
Product ID : STM32 BOOTLOADER
Serial number : 375B33653331
Firmware version : 0x011a
Device ID : unknown
===== STLink Interface =====
-------- Connected ST-LINK Probes List --------
ST-Link Probe 0 :
ST-LINK SN : 54FF6F064971545041372487
ST-LINK FW : V2J33S0
-----------------------------------------------
===== UART Interface =====
Total number of serial ports available: 0
--- wb55.dongle & wb55.nucleo ----
marek@marek-desktop:~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin$ ./STM32_Programmer_CLI -l
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
===== DFU Interface =====
No STM32 device in DFU mode connected
===== STLink Interface =====
Error: No ST-Link detected!
===== UART Interface =====
Total number of serial ports available: 0
2019-07-10 10:21 AM
A new devboard works without any problems.
2019-10-07 01:14 PM
Hi,
have you found a way, how to update Co processor without USB? Is it possible to access it from SWD/JTAG?
Thanks!
2019-10-10 04:51 AM
same issue here, boths seem dead. Boards are the preview ones I got in one of ST workshops
2019-10-20 10:18 AM
Hi! I got same issue today. After removing old coprocessor FW i was not able to detect board by USB in DFU mode. I have custom board. Port LPUART was connected via USB-serial to the PC.
I have removed FW without any issues:
But after that - i was receiving message - USB device not detected.
I made next steps and board was able to be detected via USB:
1 - Erased FLASH in normal mode;
2 - Erased FLASH, sector by sector after booting in DFU mode (with boot0 signal)
3 - Disconnect USB-Serial port, connected to the PC.
Now board works OK! Hope this post helps you.