2019-12-18 01:15 PM
I have TrueStudio v9.3.0, Stm32CubeProgrammer v2.0.0 and cubeMX ver5.2.0 installed. I can open and compile the hand-on project of BLE_HeartRate on TrueStudio but can't debug it.
console shows: "Target no device found", error in initializing ST-link device.
open cubeProgrammer also has error of "No STM32 target found".
I can do nucleo board st-link fw upgrade/downgrade via cubeProgrammer, and PC usb driver shows "ST-Link Debug"
current my nucleo board st-link fw is V2J35M26.
Need help to make the board working with TrueStudio.
Thanks in advance.