[STM32WB55] Launch app after FUS/BLE stack update without power cycling
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-26 7:53 AM
Hi,
I am working with a STM32WB55 MCU connected using a STLINK probe (SWD).
In the flashing flow, I use STM32_Programmer_CLI to erase the device, put it in FUS mode, update the FUS, update the BLE stack image, and then flash the app image.
One thing I realized was that after those steps, I couldn't start the app image without powering off and on the device. No reset, hardrst, core_rst nor anything I could find in the
STM32_Programmer_CLI --help
command allowed me to launch my app.
Is there any way to launch the app without having to manually power-off and on the board?
Is it quite annoying to have this extra step in the flow!
Kind regards,
A.P.
- Labels:
-
ST-Link
-
STM32CubeProgrammer
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-05 2:39 AM
Hello,
According to UM2237, you can use the start command (see part 3.2.7) which enables execution of the device memory starting from the specified address.
Best Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-08 8:57 AM
Hi Rémy,
Thank you for your answer.
Unfortunately, this doesn't work either!
Here is the output I receive:
$ STM32_Programmer_CLI -c port=swd sn=$MY_SN --start 0x8000000
-------------------------------------------------------------------
STM32CubeProgrammer v2.13.0
-------------------------------------------------------------------
ST-LINK SN : $MY_SN
ST-LINK FW : V3J10M3B5S1
Board : STLINK-V3SET
Voltage : 0.00V
SWD freq : 8000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled
RUNNING Program ...
Address: : 0x8000000
Application is running, Please Hold on...
Start operation achieved successfully
After this, the device never boots. If I power it off then on, it starts nicely.
The Voltage = 0.00V is not surprising as there is no Vdd cable between the probe and the device.
Kind regards,
A.P.