2024-07-23 05:09 AM - last edited on 2024-07-23 05:11 AM by Andrew Neil
I am using STM32WB55 with 32 MHz HSE and am trying to find out which input clock frequency I should use for TIM16. Unfortunately it is not clear in the diagram from the datasheet. Where can I get this information?
Greetings,
Andreas
Solved! Go to Solution.
2024-07-23 05:33 AM
Hello @AndreasC and welcome to the ST Community
the APB2 is the clock bus for the TIM16:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-23 05:11 AM
Choose a value that's appropriate to your intended use of TIM6.
The Reference Manual will detail the available options.
2024-07-23 05:25 AM
You could save yourself this answer
2024-07-23 05:33 AM
Hello @AndreasC and welcome to the ST Community
the APB2 is the clock bus for the TIM16:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-23 05:42 AM
Hello STTwo-32,
Thank you very much for the quick reply. I'm looking forward to being there
Greetings,
Andreas