2025-02-20 05:43 PM - edited 2025-02-20 05:44 PM
Hellow all,
I am running a custom BLE application on STM32WB55 and I want to run in low power STOP2 mode,At the same time, Bluetooth needs to remain in broadcasting state. I am not sure what the average power consumption is in this case. I monitored that after CPU1 enters STOP2 mode, the average power consumption is about 6mA. Is this normal? Is there a theoretical minimum average power consumption value that can be achieved when CPU1 enters STOP2 mode and Bluetooth is still broadcasting for reference? Thank you very much!