2021-07-06 5:54 AM
Hi all
Maybe you can help me understand something about the IPCC.
From my understanding: In case CPU2(BlackBox) sends the CPU1 an command:
CPU2(BLE) -----RX occupied ISR -----> CPU1(APP), look in Queue to get the user event.
: CPU1(APP) --------TX free ISR---------> CPU2(BLE) , where is the data??
When CPU1 (APP) gets a user event from CPU2, It sends a response to CPU2 in a form of TX free ISR is sent. Where is the data of that event?
Thanks.
P.s. I see that in the opposite direction the data is stored in pCmdBuffer
Solved! Go to Solution.
2021-07-19 3:05 AM
There is no BLE trace sent over IPCC. Only Thread protocol stack (and possibly Zigbee protocol) is sending traces IPCC to the M4 core.
2021-07-16 9:01 AM
The wireless stack on CPU2 never sends a command to CPU1.
It is the other way. The application running on CPU1 sends a command to CPU2 via IPCC and CPU2 returns data received from the network or answers to previous commands from the application.
Buffers used for inter-processor communication are located in SRAM2.
Attached is a basic description of IPCC.
2021-07-17 11:55 PM
Thanks,
I see that in code there are 2 ISRs for messages. Both the Async user evet and the RespCmd evnt? What is the difference?
Regarding traces, it is not possible to use the Traces Channel?
I am wondering if there is extra value in creating the channel.
Thanks.
2021-07-19 3:05 AM
There is no BLE trace sent over IPCC. Only Thread protocol stack (and possibly Zigbee protocol) is sending traces IPCC to the M4 core.