2024-07-08 05:36 AM - last edited on 2024-07-08 07:37 AM by Peter BENSCH
Hello, basically the title. What are the minimal configurations that need to be made in order for a STM device to show up into an iOS device's BLE connectable devices list without using 3rd party apps?
I currently got my app up and running and it works flawlessly using Android smartphones, but I would like to also migrate it to be able to connect to iOS devices.
Thanks!
2024-07-30 08:38 AM
Hello @tandr
I don't think this have anything to do with The BLE Technologie since it works fine in the Android Mobiles. For that I think you have to refer to one of the experimented people in this business.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.