cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 and sx1262MB2CAS Shield

AMitj.1
Associate

Hello there

I am completely new in STM32, I need to use two SX1262MB2CAS shield to tx with one of them and rx from the other one.

Do you know which drivers i will need and how to configure the stm32cubeide project to have acces to two stm32?

1 REPLY 1

Not sure I'd be using Cube, or trying this as my first outing with STM32 + LoRa

With the original LRWAN / Semtech libraries you'd need to create two radio instances to run it from a single MCU.

LoRa Point-to-Point type communications or LoRaWAN ?

If these are two separate STM32 + SX1262MB2CAS stations, perhaps look at the PingPong examples, reworking one into a Transmit only, and the other to a Receive only station.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..