cancel
Showing results for 
Search instead for 
Did you mean: 

STM LRWAN2 not working. Even with st given i-cube-lrwan package

RahulSK
Associate II

Hi All,

I have recently purchased the ST-LRWAN2 package.

I have successfully setup the LoRaWAN Gateway.

But I am not able to setup the Node device NUCLEO-L073RZ.

I am using STMCubeIDE. The software package I am using is i-cube-lrwan.

I am not able to see any output on the Serial monitor

I have attached the images for more details.

If anyone has successfully setup the device, please advice on this.

Thanks and Regards,

Rahul

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
ESchu.1
Associate II

Hello,

i use a B-L072Z-LRWAN1-board, so i make a new projekt (I-Cube) and select this board, i generate the code.

How can i use the files from I-CUBE-LRWAN firmware package (STM32CubeExpansion_LRWAN_V1.3.1). For Lorawan-example there is an Irc and Src-folder with separate main.c?

Then you must configure your node First are you using ABT or OTTA?

Wich Region you select (868Mhz for Europe)?

Greetings

E_T

Andrew Neil
Super User

A bit late, but:

"I am not able to see any output on the Serial monitor"

Note that this is to be expected: as the Getting Started Guide tells you, the ST-Link UART is disconnected from the target on the Nucleo board.

See my post of  January 20, 2021 at 12:05 PM in this thread:

https://community.st.com/s/question/0D53W00000DHlVaSAL/i-want-to-get-pnucleolrwan2-gateway-source

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Imen.D
ST Employee

Hello All,

I shared with you this post of @Andrew Neil (Community Member)​ , that contains the fixes proposed by JCOUP.

Hope this helps you !

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Note that these fixes don't make any difference to the fact that the code does not - and is not intended to - give any output to a local terminal

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.