I use the Board B-L072Z-LRWAN1 and i made o new project with Target "B-L072Z-LRWAN1". How can i now use (import) the LoRaWAN-Examle in the St32CubeExpansion_LRWAN_V1.3.1?Greetings E_T
The solution, it is my first try with this bord, the LORAWAN_APP_KEY in se-identity.h was identical with the AppKey in the TTS-Console, but the LORAWAN_NWK_KEY was differend!Another little silly thingGreetingsE_T
Hello i have the same problem: STM32WL55JC1, EndNode Example with STM32Cube IDE 1.7.0Debug:###### AppKey: 2B:7E:15:16:28:AE:D2:A6:AB:F7:15:88:09:CF:4F:3C###### NwkKey: AC:F3:EE:8D:62:23:49:3B:46:1A:B8:B1:41:EC:BE:99###### ABP ############ AppSKey: 2B...
Hello,i use a B-L072Z-LRWAN1-board, so i make a new projekt (I-Cube) and select this board, i generate the code.How can i use the files from I-CUBE-LRWAN firmware package (STM32CubeExpansion_LRWAN_V1.3.1). For Lorawan-example there is an Irc and Src-...