2024-04-10 06:59 AM
I see it has the WB55M and another WL module on it.
How is then the low power mode controlled?
Is it separate for each module?
Can I disable the other module? keep the WB55M only ?
2024-05-02 11:53 PM
Hello @DS.4
Each module is separated so you can control the low power of each alone and disable one of them to work only on the other.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-02 11:55 PM
Without more information on the specific device, it's difficult to say for sure. Here's what we can speculate:
Possible separate control: The WB55M and WL module might have independent low power modes.
Disabling the WL module: Disabling it might be possible, but proceed with caution. It could affect overall functionality depending on how the modules interact.