2018-05-08 1:04 AM
Hi,
I have some trouble getting the sigfox stack up and running on B-l072Z-LRWAN1 kit together with SDR Dongle from Sigfox, what i have done so far is:
1. Executed SignatureGenerator.bin on my device and retrieved the signature
2. Requested the PAC/ID from Murata and got the sigfox_data.h back
3. Replaced the sigfox_data.h with new data from Murata
4. Modified the sigfox stack to operate with public CMAC `SGFX_CMAC_set_key_type( CMAC_KEY_PUBLIC );`
5. Connected the dongle directly to LRWAN1 via SMA-SMA with attenuator
6. In Snek software configured the device ID and Radio configuration to match the LRWAN1 default config (RC1)
7. Tried to disable/enable authentications but no messages are coming in.
The console output is as follows:
wakeup OK
devId=009_____devPac=1______________Csenddata....F8 00 00 00 00 00 00 donesenddata....EF 00 00 00 00 00 00 donesenddata....F1 00 00 00 00 00 00 donesenddata....EF 00 00 00 00 00 00 donesenddata....EF 00 00 00 00 00 00 donesenddata....ED 00 00 00 00 00 00 donesenddata....EF 00 00 00 00 00 00 donesenddata....ED 00 00 00 00 00 00 donesenddata....ED 00 00 00 00 00 00 donesenddata....EF 00 00 00 00 00 00 donesenddata....ED 00 00 00 00 00 00 donesenddata....EF 00 00 00 00 00 00 donesenddata....EF 00 00 00 00 00 00 donesenddata....F1 00 00 00 00 00 00 doneThe blue led lits up when transmission is ongoing (LD3) while green led (LD2) blinks 6 time during that same time. Does anyone know if there are any other setting which are required to be set in order to get the messages being transmitted?
#b-l072z-lrwan1 #sigfox